10/18/2019 10:33 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating:
|
Hi jhersonjhair, the several ways to configure the communication. The best solution depends on your requirements (the amount of data, read and write from both sides, ...) The best way to start is with application example CPU-CPU communication with SIMATIC controllers (compendium). Example for the communication between CPU 1200 and CPU 300 can be found under How do you configure and program an S7 connection and the FB15 "PUT" und FB14 "GET" function blocks for data transfer between an S7-1200 CPU and an S7-300 CPU? With regards |
Last edited by: Heisenberg2 at: 10/18/2019 10:40:40 |
|
This contribution was helpful to
1 thankful Users |
Follow us on