10/21/2019 8:56 PM | |
Joined: 4/10/2017 Last visit: 2/23/2021 Posts: 32 Rating: (0) |
Hi All Firstly, need to say Im so impressed by the level of support and conduct on this forum. Very professional and helpful...thanks so much. As I delve in here...I have finished my first simple project. One thing that is not immediately obvious (although there are brief articles avaliable) is style guide/formatting etc of actually laying out the code. Would anyone possibly be willing to have a quick look over this project and comment, as tough as you want, so I can make sure Im on the way correctly? Im sure its super verbose as Im pretty green. I have programmed in a similar FB code called Pure Data/MaxMSP but its formatting is very automatic so its a little tough getting Logosoft to perform the same way. I love the way it can output the worksheets etc...but how do you turn off the green lettering? Here is the pdf Happy to include the actual project if anyone is available. Cheers AttachmentWater Dosing - LOGO Flowchart.pdf (50 Downloads) |
Last edited by: Jen_Moderator at: 10/22/2019 06:02:04Removed link and added file as an attachment. |
|
10/21/2019 9:01 PM | |
Joined: 12/18/2014 Last visit: 5/16/2024 Posts: 33043 Rating: (4082)
|
Why don't you attach the PDF file by your post? |
10/21/2019 9:57 PM | |
Joined: 4/10/2017 Last visit: 2/23/2021 Posts: 32 Rating: (0) |
The pdf text is the actual link...which you got :-)
its not the colour; its of little consequence...it was the colour denoting content...ok I see now...its actually in 2 places which is a bit confusing...also in options Ah I see, there is a layout icon but no actual menu item for it...which is also a bit confusing...UX is a bit 'additive' meaning its built upon without a well defined schema ok mulitple pages it is...so 1. is it best to just modularise to each layout and then use cut connectors or what is considered best practice? 2. Are there any examples of a well defined program based on layout rather than function. I have downloaded some of the code examples but they are fairly simple but I try some more...just if there are any pdfs showing the style guide for layout would be great 3. Is there no function to execute a 'clean up' and reroute the connections? On a per selection basis https://docs.cycling74.com/max7/vignettes/aligning_patchcords |
Last edited by: Image_Engine at: 10/21/2019 21:59:37Last edited by: Image_Engine at: 10/21/2019 22:44:57 |
|
Follow us on