11/30/2019 5:48 AM | |
Joined: 9/9/2015 Last visit: 9/30/2024 Posts: 727 Rating: (278) |
I faced this issue before. My solution is to retrieve back to the working archive and be careful when moving the runtime group. Then, always back up after successfully moving the runtime group. sometimes, the block went crazy..this issue cannot be resolved by update/reorganize. At least for my time, cannot (PCS 7 V9.0 SP1). Just recover it to the good one, then move one by one. There is another useful option, named chart based management. Always make sure you have this enabled. It can help you to organize the runtime folder automatically and you will have an extra function - Download selected CFC chart. The runtime folder is in the form of yellow colour. Blue colour folder means chart based management deactivated. If you use a blue folder, you have to do a lot of empty runtime folder deleting job. Therefore I will suggest having this function enabled. The only disadvantage is one extra FC will be created for each runtime folder (CFC chart). Loading will be increased. Hope it is helpful for you. |
Please give me 5 stars Rating if my post is helpful for you. :) |
|
Follow us on