8/17/2018 2:41 PM | |
Joined: 7/22/2015 Last visit: 4/21/2024 Posts: 23 Rating: (5) |
Hi, I'm running simulation with PLCSIM advanced, and everything is running quite fine. After a modification and a download to PLCSIM advanced, when I first run the program, I got an exception on the following line :
The exception is :
Then, if i stop the C# program and start it again, everything runs smoothly. Furthermore, the exception does not seems to be registered in the documentation. Is it a bug ? Thanks ! Ronan ----------------------------------------------------------------------------------------------------------------------------------- EDIT 04/01/2019 Problem solved by choosing to update only I/O and M bits with the following code : For the curious on the C# with PLCSIM advanced, I did a quick write up : https://www.fontenay-ronan.fr/automation-virtual-commissioning-plcsim-advanced-2-0-with-c/ |
Last edited by: Ronanf at: 1/4/2019 8:46:20 AMLast edited by: Ronanf at: 1/4/2019 8:47:44 AM |
|
8/21/2018 8:08 AM | |
Joined: 7/22/2015 Last visit: 4/21/2024 Posts: 23 Rating: (5) |
Up |
1/4/2019 8:34 AM | |
Joined: 7/22/2015 Last visit: 4/21/2024 Posts: 23 Rating: (5) |
I've just did a write up on this subject here : https://www.fontenay-ronan.fr/automation-virtual-commissioning-plcsim-advanced-2-0-with-c/ |
Last edited by: Ronanf at: 1/4/2019 8:35:17 AM |
|
This contribution was helpful to1 thankful Users |
Follow us on