8/19/2011 6:33 PM | |
Posts: 69 Rating: (0) |
Dear all, I have used PCS7 Ver6.1 + Cemat 6 for one control system. I experienced some problem with my PLC, which was 416 3DP, during dowanloading my final program. As a result, I updated my program to PCS7 V7 SP1. After this, I have one problem in my compilation (I attached the log).If I remove the check mark of creating block drivers, my problem is solved and every block (even blocks such as CH_AO) will work. On the other hand, when I mark the creating block drivers during compile, I encounter the warning that will not allow download later! Please notice that I my program was in PCS7 V6.1 and now is compilaing with PCS7 V7. In my first comlile it was convertet by program.
AttachmentLogs.pdf (274 Downloads) |
8/29/2011 11:06 AM | |
Posts: 836 Rating: (100) |
Hi, loading the HW config should solve your problem. Try to load it in PLCSIM, this should also work. |
9/13/2011 7:16 AM | |
Posts: 69 Rating: (0) |
I think we cannot download in PLCSIM. It get itautomaticallyeither from designedHWor from pre-defined CPU in PLCSIM. |
Follow us on