12/10/2019 7:08 AM | |
Posts: 9 Rating: (0) |
Hello I have Siemens 6ES7314-1AE04-0AB0 SIMATIC S7-300 CPU314 Controller, MPI, 24KB Memory as i see it have a mpi/dpi connection i have cabble also. also one in out SIEMENS 6ES7 323-1BL00-0AA0 - and power supply Siemens 6ES7 307-1KA00-0AA0 Simatic S7 Power Supply 10a 24v-dc can you help? I have it in home not in work i just trying to learn and need to understend in witch way i can put new ob remove delete on plc. i just write simple program to see if lights goes up or i have a simple two fans 12+12 volts and if it will be on not more. if i understand it after i go up with knowliges and try to write more dificult software... after i have many to learn example hmi panels software with wincc but here is noone in georgia who knows they newer give you answer :D max 10 people knows in Georgia so i need to be a 11 :) |
Last edited by: kachkachuri at: 12/10/2019 07:14:36 |
|
12/10/2019 1:12 PM | |||
Joined: 9/27/2006 Last visit: 5/14/2024 Posts: 12257 Rating: (2668) |
Hello kachkachuri; Thank you for the information on ypur system. In order to share the same terms in our explanation, you should start by reading this article, describing the S7-300 CPU memory concept: https://support.industry.siemens.com/cs/us/en/view/7302326 Your CPU corresponds to case #4 in the document, SIMATIC S7-300 CPUs and C7 Devices With MMC Bay. In your case the 24 kB referred to in your CPU description corresponds to Work Memory. But you have no Load memory, which is on the MMC that you need to insert in the memory card slot on the CPU. So you cannot dowload any block to your CPU until an MMC is provided and inserted in the PLC. The smallest size of Simatic MMC you can purchase is 64 kB,
The different MMC for your CPU are shown in this FAQ: https://support.industry.siemens.com/cs/us/en/view/9274152 The 64 kB MMC is quite sufficient for the needs of your CPU. Please do not use a MMC from a non-Siemens provider, and never try to format a Simatic MMC using your Windows OS, you would make it unreadable from a Siemens CPU. Hope this helps, Daniel Chartier
|
||
Last edited by: dchartier at: 12/10/2019 16:15:15 |
|||
This contribution was helpful to1 thankful Users |
Follow us on