12/19/2019 9:20 AM | |
Posts: 6 Rating: (0) |
I'm using TIA V15 in which through Scaling i want to show the value on scada. Pressure sensor output is given to AI module. As I'm using IW to display the value; 0 is being displayed on online simulation. Should i use PIW as I'm directly taking input from pressure sensor and how should i add PIW in program. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/19/2019 11:59:28New subject after splitting |
|
Follow us on