12/17/2019 8:37 AM | |
Joined: 5/3/2017 Last visit: 5/21/2024 Posts: 673 Rating: (217) |
Hello snowball, you can find a good description for the messages in the manual PCS 7 OS process control in the section Structure and States of Messages. And in the FAQ "What are the causes of PCS 7 control technology and system messages and what measures are to be taken to clear them? " you can find all system messages from PCS 7. A good example for the class messages is the MonAnL from the APL. The tolerance messages you can interpret as the value is not in the optimal working range. You also can config your own message systems (Configuring the PCS 7 message system) With regards |
This contribution was helpful to3 thankful Users |
12/20/2019 5:55 PM | |
Joined: 8/22/2018 Last visit: 3/2/2021 Posts: 35 Rating: (0) |
Hi Heisenberg, Thank you very much for the information. It really useful to me. with regards, snowball
|
Follow us on