11/11/2008 9:34 AM | |
Joined: 9/29/2005 Last visit: 4/26/2022 Posts: 313 Rating: (24) |
Hi, yes the set5 is customized directly for MD720-3 modem and TC65Terminal modem. You can download the library for free here.: http://support.automation.siemens.com/WW/view/en/21063345 regards Lif |
11/12/2008 4:55 PM | |
Joined: 7/15/2007 Last visit: 7/3/2024 Posts: 54 Rating: (0) |
Mr. thanks for answering my doubt, but to receive it uses the MAS5 library? Hope his comments. Atte Nelson |
11/14/2008 1:29 PM | |
Joined: 5/28/2008 Last visit: 7/15/2024 Posts: 1343 Rating: (141) |
Yes, it's the MAS5 library. Or what do you mean? |
11/18/2008 10:14 AM | |
Joined: 5/28/2008 Last visit: 7/15/2024 Posts: 1343 Rating: (141) |
Yes, you need MAS5 library to receive SMS |
Follow us on