1/3/2020 1:56 PM | |
Joined: 3/14/2008 Last visit: 7/12/2024 Posts: 2076 Rating:
|
Hi, without any software licenses, you can copy paste control module types to your plant hierarchy, you can manually change parameters in the Technological Object View under the Plant/Component view list. But it's a lot of work, the only alternative is using Plant Automation Accelerator software which you have to buy. You can then synchronize between Plant Automation Accelerator and import to and export from PCS7. See the following link for Control Module Types: |
Last edited by: Oreca at: 01/03/2020 14:04:40Last edited by: Jen_Moderator at: 01/07/2020 11:15:12Optimized link. If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on