12/29/2019 12:37 PM | |
Joined: 1/8/2014 Last visit: 1/15/2020 Posts: 1 Rating: (0) |
Hello, We are using 3VU1640-1MP00 siemens mpcb for motor of rated current of 29A. Actual current is 28A in R phase,30.5 A in Y phase, 27A in B phase. Current trip setting is set to 22A on mpcb.The mpcb is tripping after more than 10 minutes even though the actual current is 30A in Y phase. It is written on mpcb is trip current is 125% of the setting. As per setting of 22A, the mpcb should trip when current exceeds 27A. But it is not tripping. Please give me solution. Application is water pump. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/30/2019 10:49:04New subject after splitting |
|
1/7/2020 8:41 AM | |
Joined: 4/15/2009 Last visit: 10/10/2024 Posts: 126 Rating: (11)
|
Hello, Please contact the Siemens support for this inquiry directly Support Request:www.siemens.de/support-request
Best regards |
Follow us on