1/9/2020 7:33 AM | |
Joined: 3/14/2008 Last visit: 11/7/2024 Posts: 2123 Rating: (950)
|
Hi, the TLE is designed to change properties of the CMT's/EMT's/EPHT's when they are created in the master library and the instances in the project (CM's/EM's/EPH's). All parameters/signals/messages etc. that were created in the Technological I/O can be edited here. You also can change role assigments for the EM's/EPH's and other stuff.
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on