11/18/2008 8:46 AM | |
Posts: 5 Rating: (0) |
The projekt is almost done, but when i´m doing a consistency check everything seems to be in order exept for two blocks: FC1005 and FC1006 (system made blocks FC50 and FC60 for FDL communication). They both have red dots with the X, but the compiler telling me that there are 0 errors and 0 warnings (see the attached screendumps) What can I do to prevent this problem? Attachment123.zip (194 Downloads) |
11/19/2008 11:40 AM | |
Posts: 2348 Rating: (264) |
In this case you can just ask support for new version of these blocks:^) Or try these Attachmentforum_te.zip (161 Downloads) |
Last edited by: Aret at: 11/19/2008 11:45 AM |
|
11/19/2008 12:47 PM | |
Posts: 5 Rating: (0) |
Is there any corresponding blocks for FC 5 and 6 (AG_SEND, AG_RECV)? Or do I have to call Siemens? |
Follow us on