1/17/2020 2:43 PM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
Hello again Wizard, Thank you for answering. I knew how to download to Step 7 and I have already done so AS LONG AS we are talking about something in the Blocks folder (or the HW configuration). Thank you for the manual I will see what I can find in that. But I have also already download safety logic several times. BUT as we have previous concluded in this thread the Alarm texts in Danish language shown on the flex panel is coming from the PLC. IF these texts have been included in the BLOCKS folder I would have a good guess how to download them BUT they are in a "Text Libraries" folder on the same level as Sources and Blocks. So - how do I download (or in some other way implement the modified "Alarm_1_DK" file? (Please also see the screenshots where I tell you that I found the file).
|
Last edited by: xmnj at: 01/17/2020 14:44:56Spelling |
|
1/17/2020 3:02 PM | |
Joined: 4/24/2006 Last visit: 8/7/2024 Posts: 8711 Rating: (1166)
|
Hello, Have a look at the following link: SIMATIC Programming with STEP 7 V5.5 Perhaps chapter 16 might help you. Best regards, Wizard |
This contribution was helpful to1 thankful Users |
1/20/2020 11:07 AM | |
Joined: 9/30/2016 Last visit: 7/11/2024 Posts: 914 Rating: (6) |
Hello again Wizard, Thank you for answering. I have read the chapter but it doesn't quite solve my challenge. The original question have however (more or less) been answered so I will mark this thread solved and ask a new question regarding the download / transfer of the modified list.
|
Follow us on