1/21/2020 9:38 AM | |
Joined: 1/17/2020 Last visit: 5/29/2024 Posts: 22 Rating: (1) |
Good afternoon. I ask for help, I cannot understand why the window V14.0 and SIMATIC NET SOFTNET-IE S7 V14.0 demanding the license SIMATIC NET HARDNET-IE S7 V14.0 or HARDNET-IE S7 (OSD) appears. There is an engineering station, 2 servers and 3 clients (WINCC 7.4 SP1 K7.4.1.0). CPU S7-416-5H PN/DP vcommunicate via CP1623 (ISO)with servers via Named Connections . CPU 412-2-XK07-0AB0 via TCP/IP (S7-online). CPU S-1200, S-1500 via Simatic S7-1200, S7-1500 Channel (S7-online). The configuration was guided by the manual. Delivered to the license. I don 't know what to do anymore. If anyone was stalking with such a problem, please help me. Screenshots in an investment AttachmentW.docx (28 Downloads) |
Follow us on