1/24/2020 9:50 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (927)
|
Hi, State 20 should be bit 2 and 4 to be set. Bit2 means more then one command active Bit4 means: (SCT = 0 AND SCT_TAC = 0) OR (SCT = 1 AND SCT_TAC = 1) . Please check those input parameters at the SFC. |
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
Follow us on