1/21/2020 1:18 PM | |
Posts: 2 Rating: (0) |
Hi everyone, I have a TP700 Comfort HMI panel programmed, installed and licensed at site. The application program was done using WinCC2007 Flexible. Now I I have to modify something on the application program but using WinCC2008 Flexible. is there any impact on the runtime license in the HMI panel? Thanks, ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 01/22/2020 10:47:10New subject after splitting |
|
1/27/2020 7:12 AM | |
Joined: 11/15/2015 Last visit: 4/21/2024 Posts: 178 Rating: (28) |
Dear AutoGen_9808936 Have a look at this link Link Regards, |
Look for alternative not for the correct answer...if this is helping you rate it. |
|
1/29/2020 9:37 AM | |
Joined: 8/3/2009 Last visit: 4/25/2024 Posts: 12869 Rating: (1640)
|
Hello first of all a Simatic Panel like a TP700 has no Runtime licenses, only if you use special Options that need licenses. There are a few facts you have to be sure if you have transfered these special Runitme Licenses (like Audit): WinCC Flexible: https://support.industry.siemens.com/cs/ww/en/view/27005215 TIA: https://support.industry.siemens.com/cs/ww/en/view/74796111 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on