1/31/2020 8:57 AM | |
Posts: 7 Rating: (0) |
Hello, I am new to this field. I want to learn how to program siemens PLC on step7. Can some one help me with guide mark how to learn easiest? |
1/31/2020 11:28 AM | |
Joined: 9/27/2006 Last visit: 5/2/2024 Posts: 12257 Rating: (2666)
|
Hello Zlatko; In the following popular thread on the forum, Denilson Pegaia offers an excellent explanation of FBs and FCs as different types of subroutines that are used in a Step 7 program: If you only need the routine to execute once and return a result (for example a math instruction), use an FC. If your routine parameters must be available even when it is not being executed, use an FB (+ IDB, instance DB as dedicated memory block for that routine). Examples can be easily followed in this manual: Working with Step 7 https://support.industry.siemens.com/cs/us/en/view/45531551 Hope this helps, |
This contribution was helpful to1 thankful Users |
Follow us on