1/27/2020 11:18 AM | |
Joined: 6/27/2019 Last visit: 11/16/2023 Posts: 2 Rating:
|
WinCC Connectivity Pack |
2/2/2020 1:49 AM | |
Joined: 7/6/2019 Last visit: 12/27/2022 Posts: 30 Rating:
|
Hello ashadako, PV is set as an archive tag then it will be saved and old values wont get deleted . IF you want to see in a Trend View then use AOTC You can generate a report in CSV format , with all logged values along with quality code of signal , time stamp and name of the operator as well by writing VBS code |
2/2/2020 7:32 AM | |
Joined: 11/15/2015 Last visit: 6/26/2024 Posts: 179 Rating:
|
Dear ashadako How do you export as a CSV file process values displayed in WinCC Online Trend Control? Compressing of process value archives with the Swinging Door algorithm in PCS 7 How can you have a process value archived only when it changes? How is the mean value for process variables stored in the process value archive? I hope that helping you Regards |
Last edited by: Jen_Moderator at: 02/03/2020 11:17:21Optimized links. Look for alternative not for the correct answer...if this is helping you rate it. |
|
Follow us on