8/5/2008 11:09 AM | |
Posts: 60 Rating:
|
Hi Simatix, Thanks for your question. First of all please make sure that you are in fact dealing with a Profibus DP Network and not an L2 DP. So you should in fact use the IM 308C and not the IM 308B. The IM 308C is being configured using COM Profibus. I hope you have a recent copy of this program? You can read in the gsd File of the new ET200S. You can download the gsd files for the ET200S here: http://support.automation.siemens.com/WW/view/en/652154 Please read the COM Profibus documentation on how to read the new GSD files into COM Profibus. Also make sure that you use the DPV0 GSD files. You can recognize those files, because their names start with SIEM*.gsd rather than SI*.gsd. I suggest using the ET200S Compact if possible, because it is supposed to replace the ET200B and ET200L IM-SC. I hope this information is helpful. Regards, Gerard |
2/7/2020 12:19 PM | |
Joined: 9/10/2019 Last visit: 10/12/2023 Posts: 30 Rating:
|
Hi gerardammerlaan, I have ET200B modules.I wanna change with ET200S.How I can find compatibility list? How I can choose correct ET200S modules.
|
2/7/2020 3:37 PM | |
Joined: 9/10/2019 Last visit: 10/12/2023 Posts: 30 Rating:
|
profibus dp connection. I found list for ET200SP but I didnt find list for ET200B. I am searching like this list. |
Follow us on