2/16/2020 7:01 AM | |
Joined: 3/13/2019 Last visit: 9/14/2024 Posts: 154 Rating: (2) |
Dear experts, Can anybody help me on F60036 fault in sinamic dcm 6RA80. we are using sinam dcm converter with 400A output for 132kw motor,Armature rated amp 337A and field rated amp 8A,1000rpm.One incremental encoder installed for speed feedback having 1024ppr ,24v ,HTL specification. Since tomorrow we are facing F60036 fault and also output fuse which is connected in armature circuit is blowing....till now we have lost three nos semiconductor fuses...why fuse blowing drive is not tripping,???.since drive current limit is set correctly.... is my thyristor module failed??? Or something wrong with firing pcb.....hope for speedy reply.... Thankx in advance Regard's Pankaj Tiwari ------------------------------------------------------------------------------------------ |
Last edited by: pkgoluadi at: 02/16/2020 07:03:37Last edited by: Jen_Moderator at: 02/17/2020 12:34:43New subject after splitting |
|
Follow us on