2/21/2020 8:03 PM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating:
|
Hello Asad99, I hope you got necessary information in this discussion, Here is a piece of information that I would like to add to you, Regarding the usage of CEMAT Library V9.0, Yes, definitely you need CEMAT Engineering and CEMAT Server or Server redundancy, CEMAT Client licenses. Depends on your PC station architecture you need to purchase the respective licenses for the CEMAT library. kindly have a look at the attached image, shows our PC license information. We have used CEMAT server redundancy since having Hot standby. otherwise, that license will change. Then, For ES station one "CEMAT Engineering" is must and "for OS stations"CEMAT Client" is needed. Also, refer the below link having information of released license information for CEMAT V9.0 Sales and delivery approval for SIMATIC PCS 7 Minerals Automation Standard CEMAT V9.0 AttachmentCEMAT_License.zip (169 Downloads) |
Last edited by: Jen_Moderator at: 02/24/2020 09:09:13Optimized link. Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
This contribution was helpful to
2 thankful Users |
2/25/2020 5:42 AM | |
Joined: 4/28/2017 Last visit: 3/14/2024 Posts: 149 Rating:
|
Hello Asad99, i. Yes, Whatever you have conveyed regarding the CEMAT license is absolutely right. You just need a 1-Engineering and 2-Client license to your configurations. ii. The CEMAT library template made to be easy to handle the cement process and for sequential execution. If you find yourself to use it under some other application you can, Only necessity is the License. iii. Yes, If you don't want to manipulate the CEMAT library block in your logic, you can use standard blocks as well. Have a good time... |
Note: If this post did really help you, you may use the "Rate" button to express your support, Thank you. |
|
This contribution was helpful to
1 thankful Users |
Follow us on