3/7/2020 11:47 AM | |
Joined: 1/1/2017 Last visit: 7/1/2024 Posts: 331 Rating: (11) |
Dear Team, Kindly provide me the Software Compatibility Matrix from PCS7 V6.0 to PCS7 V9.1. I have gone through the link: https://support.industry.siemens.com/cs/ww/en/view/64847781 but that's not serving the total details. This link is only promoting WinCC V7.5 and it's supported packages rather than providing the required complete details of other PCS7 packages. Also provide me the Software details in the packages from PCS7 V6.0 to PCS7 V9.1 so that it'll be helpful from comparison point of view. Regards OmKris |
Last edited by: Jen_Moderator at: 03/09/2020 09:07:16Optimized link. |
|
This contribution was helpful to1 thankful Users |
3/10/2020 2:49 PM | |
Joined: 9/3/2013 Last visit: 11/3/2023 Posts: 152 Rating: (31) |
Hello OMKRIS2017, first off, these forum is from siemens, but siemens offers only the plattform for the communication between the costumers. If you have a problem with the Siemens product (software or hardware) you can contact the Siemens Support with the button "Support Request" on the every Siemens side. You find all compatibility lists here: https://support.industry.siemens.com/kompatool/pages/main/index.jsf -> Load compatibility lists -> download lists -> select under Software "PCS 7" -> your PCS 7 Version |
This contribution was helpful to1 thankful Users |
Follow us on