3/26/2020 1:21 PM | |
Joined: 8/3/2009 Last visit: 7/5/2024 Posts: 13231 Rating:
|
Hello I think you have mixed your knowledge from WinCC V7.X up with WinCC advanced... -> In WinCC Advanced you cannot do an indirect adressing but you can do Multiplexing functionality in different kinds (Adressmultiplexing, Tag Multiplexing, and address Multiplexing with symbolic adressing). If you just want to build in a Script the Tag name then you have to do it in this way: to connect strings ---------- SmartTags("blabla" & "_StringAsYouWant") = 10 then the String "blabla_StringAsYouWant" will be written with the value 10. Of course the Tag has to exist in the HMI Tags... Here are a few hints to this Topic: https://support.industry.siemens.com/cs/de/en/view/57132412 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on