4/6/2020 10:35 AM | |
Joined: 2/22/2016 Last visit: 10/6/2024 Posts: 141 Rating: (30) |
Hi good Siemens folks. This version has some new interesting features, among others it’s possible to use one mb_client to connect to unlimited number of devices. This feature is foremost intended for S7-1200 where the number of TCP connections are limited, but it may also be used for S7-1500. The API is compatible with other existing features.
As always, the library is free and can be downloaded on Github: http://github.com/rexhip/rexhip. It’s inspiring to see people start using it and to get feedback. Please contact me if you have questions, or you have a station block that you will like to add to the library. Some station blocks included:
Inside flow_meter FB:
Identical code may be used for RTU, simply by replacing the #ctrl .
|
Please use the contact form in the link below if you will like to come in contact with me. I don't check personal messages frequently. |
|
This contribution was helpful to1 thankful Users |
Follow us on