4/7/2020 11:50 AM | |
Joined: 6/12/2012 Last visit: 2/8/2024 Posts: 165 Rating:
|
Hello, I would like to add some tags to a working project but I cannot see the tags displayed on the runtime. The first two are of type float and on the S7-1200 PLC are also of type float in a not optimized database. The next two are two input bits and the last are binary tags of the same database. What is the convention to use to access this type of information? I’m using also the function: SetTagDouble(("SpBomba01"),GetInputValueDouble(lpszPictureName,lpszObjectName)); To change the tag value. Is that correct? Thanks, Bruno AttachmentTags+OPC.zip (28 Downloads) |
Thanks, |
|
Follow us on