4/1/2020 12:21 PM | |
Joined: 1/13/2019 Last visit: 7/26/2022 Posts: 4 Rating: (0) |
Dear all, Did you meet any issue with OPC UA of WinCC RT Professional Server(v15.1 + udpt4) can't get the endpoint (only Windows 10, Windows 7 without this issue). Even change port number too. I configure 2 PC(1 is windows 10, 1 is windows 7 both are in same workgroup) and running WinCC RT Professional. Windows 7's WinCC server can get & connect the endpoint by itself and also can get & connect endpoint from Windows 10 PC(both using SIMATIC OPC UA Client). But Windows 10's WinCC server can't get the endpoint by itself and also can't browse from Windows 7 PC. For Windows 10, I tried with totally fresh Windows that without other software, only have WinCC RT Pro v15.1 & Simatic NET v15.1. Is it OPC UA not support for Windows 10?
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 04/01/2020 14:09:22New subject after splitting |
|
4/9/2020 10:58 AM | |
Joined: 8/3/2009 Last visit: 10/8/2024 Posts: 13877 Rating: (1751)
|
Hello there is also another FAQ to this topic: https://support.industry.siemens.com/cs/ww/en/view/109479664 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on