4/23/2020 9:26 PM | |
Joined: 9/27/2006 Last visit: 5/5/2024 Posts: 12257 Rating: (2666) |
Hello Fabio; A few weeks ago the following discussion appeared on the forum which covered a similar question, S7-400H with WinCC Pro v15.1. A soulution was proposed, involving a Device Proxy so the S7-400H could be seen on the TIA Portal (not programmed, only seen), and scripting to switch the WinCC connection upon fail-over of the S7-400 redundant CPUs: Maybe it can be of help? Hope this helps, Daniel Chartier |
Follow us on