4/28/2020 2:03 PM | |
Joined: 8/3/2009 Last visit: 10/15/2024 Posts: 13926 Rating: (1757)
|
Hello Carlos in WinCC Professional the Taglogging is stored int he local SQL Server instance of the WinCC Professional Rutime. you cannot and should not change this. If you need the data also in other systems or another SQL Server then you have to do this manually by using scripts and an ODBC connection to another SQL Server value by value there would be no automatism. Or you need addons or Options like Industrial Data Bridge or you use scripts to read out the taglogging and write it also to another DAtabase: https://support.industry.siemens.com/cs/ww/en/view/38132261 -> the Database provider is in TIA Portal integrated so you do not need here an option. To Display Data from SQL Server into a Trend view you can use VB Script interface of the Online Trend control there is an Example (to write data from script Arrays to Control) in the WinCC v7.X Manual. Bye Murof |
Last edited by: Murof at: 04/28/2020 14:05:27If this Information really helps, you could use the Rate function |
|
Follow us on