3/12/2020 8:30 AM | |
Joined: 4/24/2006 Last visit: 7/11/2024 Posts: 8711 Rating:
|
Hello, Perhaps these links might help: How do you program communication blocks FC11 and FC12 for the PROFINET IO controller? - You need 1 call of both blocks. - You need the amount of bytes to be mapped in Datablocks. You communicate through CP. Best regards, Wizard |
This contribution was helpful to
1 thankful Users |
5/6/2020 2:10 PM | |
Joined: 3/5/2014 Last visit: 8/5/2022 Posts: 5521 Rating:
|
hi, no, you won´t. The CP343-1 has an own subordinate IO-system that needs to be read-out with the functions PNIO_SEND/PNIO_RCV. You can see it when you establish an IO-System on an internal interface(PN or PB). You can assign the address twice one on the internal system and one in the PNIO-System from the CP343-1. Whit addressing Ix.x and/or Qx.x you accessing the process-image of the IO-system of the internal interface. thats why you need to use this blocks like it is described in the FAQ: How do you program communication blocks FC11 and FC12 for the PROFINET IO controller?hope this helps, regards, |
FCK WAR! |
|
5/7/2020 9:04 AM | |
Joined: 9/14/2017 Last visit: 12/1/2022 Posts: 13 Rating:
|
SO do I need to make a DB with an array of 528 byte? Why does it need so much? |
Follow us on