2/16/2019 6:37 AM | |
Posts: 1 Rating: (0) |
A huge thank you for the support of older systems. Could I ask if there is an easy way to get the software to run on a modern laptop? Do I need to resurrect an old winXP machine, or run an emulator on a Xubuntu machine, or can I get a reliable DOS emmulator for a Win7/Win10 laptop? Does the TI PLC require a serial connection, can I use a USB to serial adaptor? My main goal is to get the ladder out of an existing PLC and work with the input/output list and logic to get it onto something modern. Am I reaching for the stars? Again, many thanks. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/18/2019 7:28:24 AMNew subject after splitting |
|
5/4/2020 11:45 PM | |
Joined: 3/21/2019 Last visit: 8/27/2024 Posts: 3 Rating: (0) |
As a further comment about your Xubuntu machine, the debian/ubuntu repositories do contain the DOSbox emulator. I've used it with Ubuntu, and I've used it with Raspbian on the raspberry pi. TIsoft runs well. On the rPi, it works much faster on a Pi 4 of course, but speed is acceptable on a Pi 3. I have successfully used the UART to go online from a Pi 2 to the TI545. ( I didn't do it on a Pi 4 because I'm using that computer for other tasks.) |
5/12/2020 11:08 AM | |
Posts: 2 Rating: (0) |
I know DOSBox provides emulation of old systems in which you can install an old program. Give it a try. |
Follow us on