5/26/2020 12:38 PM | |
Joined: 5/12/2006 Last visit: 7/8/2024 Posts: 22299 Rating:
|
Hello, is not possibel to open a V14(SP1) project in V15(or higher) if S120 Drives are in the project https://support.industry.siemens.com/cs/ww/en/view/109755173 Regards Christoph |
This contribution was helpful to
1 thankful Users |
5/26/2020 12:48 PM | |
Joined: 10/26/2012 Last visit: 4/24/2024 Posts: 56 Rating:
|
Hi Christoph. Is there a workaround for the issue described by the original poster? The reason for the project failing to open ,is it due to hardware not being compatible with v15 (or Higher)? Could you perform a device replacement as an example and then try to migrate/open the project with V15 (or higher)? |
Follow us on