5/27/2020 10:40 AM | |
Joined: 9/17/2015 Last visit: 2/8/2024 Posts: 7 Rating: (0) |
Thanks for your quick answare. Other question, if i have two PLC in the same net, connected to one PC, is it posible to open two different istance of WINCC (i use wincc advance rt), one connected to PLC1 and the other one to PLC 2 and eventually to show the two WINCC in an connected monitor with the extended desktop? thank you ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 05/27/2020 12:24:58New subject after splitting |
|
5/27/2020 12:07 PM | |
Joined: 2/5/2013 Last visit: 5/9/2024 Posts: 320 Rating: (74) |
Just suggestion for WinCC Advanced Create a single project . Create Connection for both PLC Controller in HMI connection. Copy respective Tags,Screens,Alarms,Data Log for respective controller in single project. Check below FAQ How do you use multiple monitors simultaneously with the WinCC (TIA Portal) Runtime Professional? Multiple monitor is possible with WinCC Professional. Even though you have to create single project. I hope this will be helpful to you. Br, |
Please rate it. |
|
Follow us on