6/30/2020 3:49 PM | |
Joined: 8/3/2009 Last visit: 8/6/2024 Posts: 13467 Rating: (1704)
|
Hello for example LINK (Its also Possible in VB Script and also with WInCC Professional in the same way) If you want to know a specific SQL Statement I would use the Edit dialog in Runtime and use a Little help Script to print out (MSGBox for example) the SQL filter statement that you have "clicked together" . If you want to edit it hardcoded you also can set it in the Properties of the Control. Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on