6/29/2020 2:08 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, Aiii, using WinCC duplicator should not be used on PCS7. Sounds like Step7+WinCC engineers who happen to program in PCS7 the Step7 way. But OK, The OS project is created on the master server. When a OS standby server is created, it can be set as standby server in the OS project settings on the ES. For this, a WinCC Application Stby must be inserted as well in the hardware settings. Make sure that is checked in order. When downloading, you right click on the master server and hit PLC->Download. When downloaded changes can be done (in some cases you need a full download), the master server will be downloaded and after user confirmation, the standby server is downloaded one by one. If you can only do a full download, you must exit runtime on one server (and best to close WinCC project as well) and right click on the server you want to download in the ES project. After the download is done, you can put the server back in runtime. In my experience, I always restart the server prior to restarting WinCC runtime, just to be sure. When the server is in runtime, please check if the synchronization has been completed, meaning the data is synchronized. This is an alarm in the Process Alarms list something like: End of synchronization/ Completed. After that (which can take up 5-10 minutes in some cases), exit runtime on the other server and repeat the procedure for this server.
|
Last edited by: Oreca at: 06/29/2020 14:14:18Last edited by: Oreca at: 06/29/2020 14:16:13If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
6/29/2020 2:16 PM | |
Joined: 3/13/2015 Last visit: 5/2/2024 Posts: 123 Rating: (38) |
Apparently Oreca and I where trying to help at the same moment |
Last edited by: Molthoff at: 06/29/2020 14:16:51 |
|
6/29/2020 2:17 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Two useful answers...fabioga66 is lucky today
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to1 thankful Users |
6/29/2020 3:23 PM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Haha Yes that is possible to do, but you need to configure the VMsettings properly at least. |
Last edited by: Oreca at: 06/29/2020 16:23:50If I could help you, you can use the RATE button. Thank you. |
|
Follow us on