12/21/2017 3:03 AM | |
Posts: 1 Rating: (0) |
HI All, I'm new with TIA portal. Platform: Software: TIA Simatic STEP 7 portal V13 (V13_SP1_Upd9) PLC to communicate with: CPU 1212C, 212-1AE31-0XB0 over profinet I'm able to connect with PLC either through detect option or via Add new device with specific model and get the PLC online, but when I'm uploading the program it gives following error. "Loading will not be performed because preconditions are not matched" & another error underneath to this message is "one or more blocks cannot be uploaded from the device" I have attached the word file where it can be easily viewed, can someone guide how to find that which of the specific precondition is not matched? is it the blocks error which shows under that message or what? how to exactly know what to fix? Thanks
AttachmentSnapshots for -HMI-1.zip (68 Downloads) |
Last edited by: Jen_Moderator at: 12/21/2017 2:20:08 PMAdded attachment as a ZIP file. |
|
This contribution was helpful to1 thankful Users |
7/15/2020 12:23 PM | |
Posts: 1 Rating: (0) |
same probem face. |
Follow us on