12/9/2008 11:05 AM | |
Posts: 42 Rating: (0) |
Hi We have a problem using TP 177B and WinCC flexible 2007.. The problem is next.... Attachmentexample of administration.pdf (153 Downloads) |
12/9/2008 11:36 AM | |
Joined: 5/8/2006 Last visit: 4/19/2024 Posts: 1085 Rating: (77) |
Hi, does the panelfreezed generally or doesn't workonly the access to protected area? Do you use password aging? Bye |
12/9/2008 2:04 PM | |
Joined: 4/24/2006 Last visit: 4/26/2024 Posts: 8616 Rating: (1147) |
Dear Miki Rapaic, You did not mention, but I guess you are using WinCC flexible 2007 + HF4. If not, you can download hotfix 4 from this link: http://support.automation.siemens.com/WW/view/en/28882233 Have you already performed an OS update, with option 'Reset to factory settings'? Have a look here, how to perform: http://support.automation.siemens.com/WW/view/en/19701610 Best regards, Wizard |
12/9/2008 2:06 PM | |
Joined: 5/8/2006 Last visit: 4/19/2024 Posts: 1085 Rating: (77) |
Hi, if you get the system message which is described in the following FAQ you type in 3 timesan incorrect password. (Note the fifth point in the following FAQ): http://support.automation.siemens.com/WW/view/en/24456113 Do you know thegeneral tipsin the followingFAQ? http://support.automation.siemens.com/WW/view/en/24140534 Bye |
Follow us on