8/19/2020 6:36 AM | |
Posts: 83 Rating: (0) |
Hi Chris, I have winccflex intergrated with S7PLC. Can you tell me step by step how to migrate? Thanks
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/19/2020 07:44:51New subject after splitting |
|
8/19/2020 7:45 AM | |
Posts: 83 Rating: (0) |
Using Ethernet. I can ping to panel. Transfer mode is in Ethernet channel. |
8/19/2020 7:48 AM | |
Posts: 83 Rating: (0) |
Ethernet. Set transfer channel to Ethernet. Can ping to device IP |
8/19/2020 7:53 AM | |
Joined: 5/12/2006 Last visit: 11/11/2024 Posts: 22439 Rating: (3029) |
hi, panel displayed in accessible nodes? |
8/19/2020 8:03 AM | |
Joined: 5/12/2006 Last visit: 11/11/2024 Posts: 22439 Rating: (3029) |
and then click on yes, what happen? |
8/19/2020 8:28 AM | |
Posts: 83 Rating: (0) |
It does OS update and I transfer the program. It seems working now. Thanks Chirs |
This contribution was helpful to1 thankful Users |
Follow us on