1/1/2018 2:54 PM | |
Joined: 2/15/2012 Last visit: 4/11/2024 Posts: 56 Rating: (12) |
Hello everyone, I have made a tool that converts a .rdb logfile into a .csv file. When you are logging in TIA or wincc flexible, you can choose to log you data into a .rdb file. When you need that data to use it in excel, you must use copy instructions inside your runtime project, this is not always so easy. You can download the tool here: RDB2CSV This is for demo purposes or educational use only. When using this software, it is at you own risk. (It's just a hobby project.) Note that the logging structure can also be modified in future releases by Siemens, so that the dataprocessing isn't correct anymore. Please feel free to post comments and feedback so I can improve this. Kind regards, Tim. |
Last edited by: coldrestart at: 1/1/2018 3:05:01 PM |
|
This contribution was helpful to13 thankful Users |
3/26/2018 6:32 AM | |
Joined: 5/30/2016 Last visit: 3/6/2024 Posts: 2 Rating: (0) |
Thank you very much, you saved my life!! |
This contribution was helpful to1 thankful Users |
8/25/2020 10:39 AM | |
Joined: 8/6/2015 Last visit: 10/9/2023 Posts: 10 Rating: (1) |
Awesome tool! Thank you so much for sharing!! |
Follow us on