9/17/2020 3:13 PM | |
Joined: 6/19/2019 Last visit: 9/5/2024 Posts: 697 Rating: (73) |
In my mind somethere must be time synchronization. Maybe this PDF will help you. |
Last edited by: Mr.V at: 09/17/2020 15:18:41 |
|
9/17/2020 4:27 PM | |
Joined: 9/9/2015 Last visit: 9/25/2024 Posts: 727 Rating: (278) |
I guess something wrong with your timesync. 1. Ensure the other CPU timesync function normally, try trigger one alarm of the CPU and observer the time, comparing with OS server time. 2. If the other CPU is okay, compare the CPU Time Sync settings with the rest of CPU.
|
Please give me 5 stars Rating if my post is helpful for you. :) |
|
This contribution was helpful to1 thankful Users |
9/18/2020 7:07 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating: (2166) |
Hello Sibthorpe88, it depends if you use Bit-messaging or chronological messaging. see FAQ: https://support.industry.siemens.com/cs/ww/en/view/23730697 In the case of chronological messaging, the wrong timestamp is In the case Bit-messaging the timestamp is set from the systemtime Regards Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
Follow us on