9/23/2020 7:40 AM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Hi I have installed three PCS7 version (v8.0 SP2, v8.2 & v9.0 SP1) on the three systems with win7 64bit. Based on the logic requested, I need the diverter function block. As indicated in the attached document, I have to use FB1127 (VlvDiv - Diverter valve) from PCS 7 Industry Library, but unfortunately I could not find the download link for this library or FB1127. Can anyone guide me? AttachmentAttachement.zip (86 Downloads) |
9/23/2020 8:00 AM | |
Joined: 3/14/2008 Last visit: 10/15/2024 Posts: 2111 Rating: (942)
|
Hi, First of all, you cannot find any downloads on the Siemens site for PCS7 V8.0. (same goes for PCS7 V8.1). It has become a legacy product meaning there is no more support, you will need a Legacy System Service Contract. It is therefore recommended to upgrade to at least PCS7 V8.2. Contact your Siemens Sales person for information about this contract.. The Industry Library must be purchased: PCS7 Industry Library V8.0 order information (Legacy product!) PCS7 Industry Library V8.2 order information PCS7 Industry Library V9.0 SP1 order information Updates for the IL library can be download free of charge from Siemens. See my thread: PCS7 Complete Overview under tab: Software updates Regards, Sandor |
Last edited by: Oreca at: 09/23/2020 08:04:58If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to2 thankful Users |
9/23/2020 6:16 PM | |
Joined: 12/16/2018 Last visit: 6/16/2024 Posts: 67 Rating: (0) |
Hi Mr. Oreca Thanks a lot for your guidence as anytime |
Follow us on