Industry Online Support
Technical Forum
9/24/2020 4:08 PM | |
Joined: 9/14/2018 Last visit: 4/7/2024 Posts: 3 Rating: (0) |
My ET 200 motor starters Part number 3RK 1308-0CC00-0CP0 do not reset each time a motor or imbalanced power fault is detected by the motor starters. I thought this version of motor starters are fail safe and should reset once the fault acknowledgment button is pressed or when the power supply is switched ON/OFF. I have upgraded the device firmware to the latest version in vain. It is getting very expensive since each time the motor starter get stuck in fail safe mode , I must replace with a new motor starter. Can someone help? I have attached the diagnostic log book. ------------------------------------------------------------------------------------------ AttachmentA500 Diagnostic log book.pdf (102 Downloads) |
Last edited by: The Helping Hand at: 09/25/2020 12:10:27New subject after splitting |
|
Follow us on