9/13/2020 4:57 AM | |
Posts: 3 Rating: (0) |
Hi friends, I'd like to know if there is a way for communicate an S7-1500 with CP1543-1 with a ISO Transport Protocol to an application of Wincc V7.5 SP1. I have configured the channel connection, I've set the PG/PC interface to work with ISO protocol, however I dond't now if I have to do something else in S7-1500 more than enable "Use ISO Protocol" and setting the mac address. I'll appreciate your help. Thank you. ------------------------------------------------------------------------------------------ |
Last edited by: The Helping Hand at: 09/14/2020 16:16:55New subject after splitting |
|
9/27/2020 5:14 PM | |
Joined: 12/12/2011 Last visit: 12/30/2020 Posts: 821 Rating: (40)
|
Hi, Have you installed a compatible version of simatic net? See the link: https://support.industry.siemens.com/kompatool/pages/main/index.jsf B.R. |
Grundkurs/Systemkurs WinCC V7: |
|
Follow us on