9/30/2020 11:14 AM | |
Joined: 4/13/2016 Last visit: 6/22/2022 Posts: 12 Rating: (0) |
Dear Mr. Chartier, I have a same question in this regard, i am currently working on a project and i need to extend one rack (IM153-2) , in my hardware configuration i am unable to find the new module supplied by siemens as (153-2BA10-0XB0) . I went through different threads on this forum and came to know that either i can update my hardware catalog or i can use the existing configuration as 153-2BA10-0XB0 is the modified form of the 153-2BA02-0XB0 and compatible. I configured it but in diagnostics its showing an error as "inserted and configured module types are not the same" . I tried to find and upload GSD file but it only has ET-200M but not the 153-2BA02-0XB0 in the drop down list. I also tried to download / manual update the hardware updates but no luck either. Screenshots are attached. Kindly suggest me the way forward please. Step 7 Version: 5.5+SP3 Revision level: K5.5.3.0 Thanks and regards, ------------------------------------------------------------------------------------------ AttachmentScreenshots.pdf (132 Downloads) |
Last edited by: Jen_Moderator at: 10/01/2020 07:33:51New subject after splitting |
|
Follow us on