10/2/2020 7:34 AM | |
Joined: 3/14/2008 Last visit: 4/26/2024 Posts: 2066 Rating: (928)
|
Hi, The MsgEvId will get the value because system attributes are assigned to it. 1. S7_server := 'alarm_archiv" 2. S7_a_type :='alarm_8p' The S7_server makes sure the compile calls necessary options like assigning message numbers and archive numbers. The S7_a_type defines the block which is sending the data (alarms). The message system will use this to determine the message block that must be used. |
If I could help you, you can use the RATE button. Thank you. |
|
10/2/2020 8:57 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hi PCS7_dude, in addition to Oreca, in the FAQ What should you watch out for if you want to call two ALARM_8P blocks in a function block? you can find a SCL-source how to integrate an ALARM_8P in your own block. With regards |
Follow us on