9/30/2020 5:47 PM | |
Joined: 2/10/2015 Last visit: 4/10/2024 Posts: 285 Rating: (1) |
Hello everyone, I have a wincc flexible 2008 project that I want to migrate with tai v13 sp1 but, when I start the migration with tia portal, I perceive the faults 1 and 2. When I resume again I perceive the fault 1 and 3. the original wincc project was edited with an earlier version and I have wincc flexible 2008 sp5, I opened the project with wincc and with the option "copy project step7" I made the copy but when I start the migration fault 1 and 3 still appear. I need your help to solve this problem because the console of a production line is out of service and I have another console with which I want to replace the one that is out service.see attached.thank you for helping me. receive my best regards.
Attachmentfault.zip (194 Downloads) |
10/5/2020 10:15 AM | |
Joined: 8/3/2009 Last visit: 4/18/2024 Posts: 12813 Rating: (1633)
|
Hello Franck Herve Perhaps this FAQ can help: https://support.industry.siemens.com/cs/de/en/view/109486003 You can also try to di the Migration of the WinCC flexible Project in two steps with the Migration Tool: https://support.industry.siemens.com/cs/de/en/view/58638200 Bye Murof |
If this Information really helps, you could use the Rate function |
|
Follow us on