10/6/2020 9:23 AM | |
Joined: 3/30/2020 Last visit: 7/17/2024 Posts: 4628 Rating:
|
Hi Kal. I am missing detail of your program which makes it difficult to make any comment. Let me show you a simple program that I have prepared for you. One uses OB30 and the other uses OB20. Try to replicate the results first. I did not have a PLC, so I simulated an S7-1200 FW4.3 in PLCSIM V15.1. It is not uncommon that the simulated results will be a few milliseconds off. BR Attachmenttime-cycle-interrupt.zip (113 Downloads) |
Last edited by: qwazee at: 10/06/2020 09:24:25Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
10/7/2020 4:13 AM | |
Joined: 3/16/2015 Last visit: 10/10/2021 Posts: 1250 Rating:
|
Thanks gentlemen. Putting the instruction in OB100 would beat the purpose as I would like to change in the program. Attached is an archive in version 15.1 for an s7-1200 FW4.3 and it is pretty much as descried, very simple, just SET_INT instruction executed in interrupt OB40 by a digital input rising edge ; I also placed it in OB1 with a rising edge tag and of course the result was the same. The first execution is random, usually between 2-3 seconds after instruction execution and once I got it just over 5 seconds. Thanks Kal AttachmentTimed_CyclicInterupt.zip (99 Downloads) |
Last edited by: Kal.A at: 10/07/2020 04:18:51 |
|
Follow us on