9/30/2020 3:20 PM | |
Joined: 7/30/2014 Last visit: 4/16/2024 Posts: 145 Rating: (1) |
Hello I have a project with a server / engineer (single station) where I added an OSC13 operator station I made the necessary configuration adding the general IE card the IP address and the MAC address. I affected the OS13 server the problem is that when I run the configuration of the target system (target system ---> configure) I get the error message "cannot access the target computer" knowing I have defines the path of the target computer. In NCM I found general IE message cannot convert an SDB. AttachmentNouveau Document Microsoft Word.docx (42 Downloads) |
10/1/2020 8:44 AM | |
Joined: 5/3/2017 Last visit: 4/19/2024 Posts: 673 Rating: (216) |
Hello sam2014, for a OS Client you don't have to configure a "IE General" and it's not necessary to configure the PC Station. For a OS Client you only have to add the path to the OS Client and assign the OS Server. If you create a new multiproject in PCS 7 I would recommend you the manual PCS 7 Compendium Part A - Configuration Guidelines, there you can find a step for step instruction to create a PCS 7 multiproject. With regards |
This contribution was helpful to1 thankful Users |
10/1/2020 10:02 AM | |
Joined: 7/30/2014 Last visit: 4/16/2024 Posts: 145 Rating: (1) |
Thank you for the reply I had to redo the work from zero if I have other problem I put you in picture. only for the server I have to put the load path of the target computer or not Thanks |
Last edited by: sam2014 at: 10/01/2020 10:06:34 |
|
10/1/2020 11:52 AM | |
Joined: 7/30/2014 Last visit: 4/16/2024 Posts: 145 Rating: (1) |
Thanks for reply I added my operator station again I assigned my server and defined my load path I compiled and started the load here is the translation: 10/01/2020 10:19:07 AM: The entire WinCC project will be transferred to the OS Runtime. AttachmentLOAD.txt (54 Downloads) |
Follow us on