1/31/2012 11:51 AM | |
Posts: 3037 Rating: (192)
|
Hello, You cantest with the lifebit with your plc programwhether the connection still exist to panel. you can find more information about the areapointer coordinationin the following manual. See in the chapter 9.11.5.4 ---> Areapointer coordination WinCC Advanced V11.0 SP2 Tweety |
This contribution was helpful to2 thankful Users |
10/8/2012 12:07 PM | |
Posts: 3037 Rating: (192)
|
Hello Heberto_hbo, I found this example which you can visualize the satus of the CPU at operator panel. You can see a description and a project of this for WinCC flexible. If you have WinCC flexible 2008 SP2, then you can migrate this projectto WinCC V11. How can you visualize the current status of the CPU on a WinCC flexible operator panel? Tweety |
This contribution was helpful to1 thankful Users |
Follow us on