10/17/2020 11:48 AM | |
Posts: 2 Rating: (0) |
Hi qwazee, I don't have access to the physical HMI at the moment and I'm unlikely to until getting to the FAT stage of the project. I'm anxious that I don't want to get to this stage and then have to look at changing all the fonts because they aren't displaying correctly. I'm using SIMATIC STEP 7 Professional - WinCC Advanced V15.0, I've also attached a screenshot detailing all of the products I have installed. I've also attached an example project which is giving me the issue. It is a new project with just the KTP400 added and the varying text sizes placed on the root screen. Thanks, Daniel AttachmentFontTest Program & Installed Software Versions.zip (52 Downloads) |
Last edited by: DanHitch at: 10/17/2020 11:49:37 |
|
Follow us on